Does the EH1512 series enclosure provide power to the IX or IXE Sarix series camera

Issue

Can I use an EH1512 series enclosure to power the IX or IXE Sarix series camera?

Product Line

Pelco Cameras

Environment

  • Sarix IX/IXE Series
  • EH1512-1 Series

Cause

Compatible Enclosure for Sarix IX/IXE box cameras outdoors.

Resolution

Yes , but only the EH1512-1 models. The EH1512-1 provides an output voltage of 24 VAC for Camera Power.

Note: The -2 and -3 models will not power the Sarix IX and IXE series cameras. 


Click Here for view of additional housings that fit Sarix Box Style cameras.