What is the maximum safe input voltage for a Camclosure 2 Integrated Camera System?

Issue

What is the maximum safe input voltage for a Camclosure 2 Integrated Camera System?

Product Line

Pelco Cameras

Environment

  • IS50 Series
  • IS20 Series

Cause

Voltage input tolerance of Camclosure 2

Resolution

The Camclosure 2 Integrated Camera System supports 24vac with a 10% +/- allowable variance; therefore 26.4 volts is the maximum allowable input voltage.
 

*IS20, IS21, IS50, IS51, volts, vac