Start a sequence on a CM6800 Series Matrix using the KBD960 Series Joystick Keyboard.

Issue

How to start a sequence on a CM6800 Series Matrix using the KBD960 Series Joystick Keyboard.

Product Line

Pelco Matrix

Environment

  • CM6800 Series
  • KBD960

Cause

Steps to start sequence view

Resolution

STARTING SEQUENCES

You can start a sequence from Main Menu 2 or from the Sequence Menu:

  1. Go to Main Menu 2.
  2. Enter a sequence number (1-16).
  3. Select SEQ

or

  1. Go to the Sequence Menu.
  2. Select the UP or Down to scroll through available sequences.
  3. Select Right or Left arrow