Adjust On-Screen Label Display for Esprit Series Integrated Positioning Systems

Issue

How to adjust On-Screen Label Display for Esprit Series Integrated Positioning Systems?

Product Line

Pelco Cameras

Environment

  • ES30C Series
  • ES40 Series

Cause

Programming of text position

Resolution

The Esprit Series OSD Labels can display AZ/EI Direction, Direction, and Zoom
To toggle these OSD Labels on or off, you must first access the Cameras' Preset 95 Menu. To begin, please refer to Lessons Learned Article #11245: "Preset 95: Accessing Esprit Main Menu"

Once you've accessed the Cameras' Preset 95 Menu, perform the following steps:

  1. Press 95 then press and hold Preset. Main menu appears.
  2. Move joystick to “Other” and press Open or the Open Iris (+) button.
  3. Move joystick to “AZ/EI Direction” and press Open or the Open Iris (+) button.
  4. Move joystick to the desired OSD Label Item and then press Open or the Open Iris (+) button.
  5. Move joystick up or down to Toggle between On/Off as desired and then press Open or the Open Iris (+) button.
  6. Repeat steps 4 and 5 for each desired OSD Label adjustment.
  7. When Finished, move joystick to “Exit” and press Open or the Open Iris (+) button.