Playback an exported video clip from a DX3100 Digital Video Recorder.

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

How can I playback an exported video clip from a DX3100 Digital Video Recorder?

Product Line

Pelco Video Management

Environment

DX3100 Series Digital Video Recorder

Cause

Video file exported from DX3100 requires the DX3100 Remote Client software.

Resolution

Download and install the DX3100 Remote Client software. Open the DX3100 Remote Client after installation and follow the steps below.

  1. Click the Connect button in the Remote Client software to bring up the Site/File Open window.


     
  2. Locate and select the Local tab.


     
  3. Click the Browse button and locate the recorded video files, then press Open.


     
  4. Press the Add button to add the file for playback.



     
  5. Highlight one or multiple files in the local window and click OK, this will bring up the main screen with the video displaying.



    During LOCAL playback of recorded video, you can pause play in order to print a hard copy or save an image file to disk. You can also search a video file being displayed from the STOP or PAUSE position by using the controls located to the right of the main screen: PLAY, PAUSE, ONE FRAME FORWARD, FAST FORWARD, and FAST BACKWARD.