What are the zoom limits on the Spectra IV Series?

Issue

What are the zoom limits on the Spectra IV Series?

Product Line

Pelco Cameras

Environment

  • DD4TC16
  • DD4CBW
  • DD4C22
  • DD4CBW23
  • DD4CBW35

Cause

Zoom capability for viewing.

Resolution

Zoom limit allows the user to define a limitation on the amount of telephoto zoom. The settings vary depending on camera model.

  • 16X (Models DD4TC16 and DD4TC16-X)
  • 18X (Models DD4CBW18 and DD4CBW18-X)
  • 22X (Models DD4C22, and DD4C22-X)
  • 23X (Models DD4CBW23 and DD4CBW23-X)
  • 35X (Models DD4CBW35 and DD4CBW35-X)