Can I export/import the configuration settings of a DX8100 Hybrid Video Recorder using the DX Series Client?

Issue

Can I export the configuration settings of a DX8100 Hybrid Video Recorder using the DX Series Client?

Product Line

Pelco Video Management

Environment

  • DX8100 Series hybrid video recorder (HVR)
  • DX Series Client

Cause

DX Series Client Software does not support the feature.

Resolution

No. User must be local to the DX8100 system or use the DX8100 Client software to export/import the configuration settings.  The DX8100 Client though is not supported with Windows 7 or newer.