Will the CM9760-CDU-T Code Distribution Unit communicate with 3rd party Digital Video Recorder using RS-422 data?

Issue

Will the CM9760-CDU-T Code Distribution Unit communicate with 3rd party Digital Video Recorder using RS-422 data?

Product Line

Pelco Matrix

Environment

  • CM9760-CDU-T Code Distribution Unit
  • 3rd Party DVR

Cause

Use RS-422 serial communication for controlling pan/tilt or dome receivers.

Resolution

Yes. The CM9760-CDU-T Code Distribution Unit  can be used with any system that uses RS-422 serial communication.

For further information please see CM9760-CDU-T spec. sheet.