Supported export data types on the DX Series Client

Issue

What are the export data types on the DX Series Client?

Product Line

Pelco Video Management

Environment

DX Series Client

Cause

Available Export options

Resolution

Export data types: Data is exported in either AVI or Native format. AVI is the default format.

NOTE: DX Series Client will not export video from the DX4000 Series DVR.

  • AVI: You must use a viewer such as a Windows ® Media Player ® to view this data.
  • Native: Use the DX Series export Viewer to view this data.