What is the pinout for the RS232/422/485 serial interface port on PelcoNET NET300/NET350 Receiver and Transmitter?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

What is the pinout for the RS232/422/485 serial interface port on PelcoNET NET300/NET350 Receiver and Transmitter?

Product Line

Pelco Transmission & Power

Environment

PelcoNET NET300/NET350 Receiver and Transmitter

Cause

For the PelcoNET to communicate with each other the wires need to hook up to the correct pins.

Resolution

The pinout PelcoNET NET300/NET350 Transmitter and Receiver RS232/422/485 serial interface port is determined by mode selected when configuring the device.
 

Pin RS-232 RS-422/485
1 DCD (data carrier detect) -
2 RX (receive data) RX+ (receive data plus)
3 TX (transmit data) TX– (transmit data minus)
4 DTR (data terminal ready) -
5 GND (ground) GND (ground)
6 DSR (data set ready) -
7 RTS (ready to send) TX+ (transmit data plus)
8 CTS (clear to send) RX– (receiver data minus)
9 - -