What is the power requirement for the Outdoor Spectra IV series?

Issue

What is the power requirement for Spectra IV series?

Product Line

Pelco Cameras

Environment

Spectra IV environmental series

Cause

Product Specification - Spectra IV with heater will drain more voltage when the heater is turn ON.

Resolution

  • The Spectra IV requires 24 VAC at 73 VA (73 watts) 3.04 Amps (with heaters) and 23.04 VA(23.04 watts) .96 Amps (without heaters).
  • Use of 24 VDC requires 3 AMPS, 72 watts (with heaters) and  0.7 amps, 16.8 watts (without heaters) Any power supply that meets these requirements may be used.

See LL#8675 for recommended power supply.