Will the Endura NET5301R Decoder work with streams from an Endura NET5401T Encoder?

Issue

Will the Endura NET5301R Decoder work with streams from an Endura NET5401T Encoder?

Product Line

Pelco Video Management, Pelco Transmission & Power

Environment

Endura NET5301R Decoder- All versions
NET5401T Encoder- All versions

Cause

The video compression formats from NET5401T is different so the NET5301R cannot decode the compressed video.

Resolution

No. The Endura NET5301R Decoder will not decode h.264 streams, only MPEG-4. The decoder will only work with the NET5300 Series.