Remote CM9760-KBD Intelligent Keyboard has no power.

Issue

The CM9760-KBD Intelligent Keyboard Power Supply is not installed at the remote location.

Product Line

Pelco Matrix

Environment

CM9760-KBD Intelligent Keyboard
PS01-3002-9015G or CM95905UPS Keyboard Power Supply

Cause

The CM9760-KBD Intelligent Keyboard is located to far away from the Keyboard Power Supply.

Resolution

The CM9760-KBD Intelligent Keyboard may be extended up to 4000ft away from the device that it controls. The Keyboards Power Supply must also be installed at the remote location, within 25ft of the CM9760-KBD.
 
For proper operation move the Keyboard Power Supply to the CM9760-KBD Intelligent Keyboard end of the remote location.
 
For further information refer to the CM9760-KBD Installation/Operation Manual.