Configure the ERD97P21-U Receiver for P protocol, Address and Baud Rate

Issue

Configure the ERD97P21-U Receiver for P protocol, Address and Baud Rate

Product Line

Pelco Cameras

Environment

ERD97P21-U Receiver

Cause

The dip switches in the ERD97P21-U receiver need to be configure per communication rate and protocol requirement.

Resolution

Inside the ERD97P21-U receiver, Dip switches are used to select the receiver address, the communication rate and protocol. The Dip Switches consist of 8 to set according to the installation requirements.

  • Switches 1, 2,3,4 and 5 configure the address setting. These switches are in Binary form plus 1.
    example:  Switches 1,2,3,4,5 all in Off position plus a value of 1 equals P address 1. 
    Switch image: View switch image here

     
  • Switches 6,7 configure the Communication Rate.  
    Communication Rate
    Switch 6
    Switch 7
             1200 Baud
    Off
    Off
             2400 Baud
    On
    Off
             4800 Baud
    Off
    On
             9600 Baud
    On
    ON

  • Switch 8 Selects P protocol.
    Protocol
    Switch 8
    Reserved
    Off
    P Protocol
    On