Call up cameras according to which multiplexer they are connected to in a two Genex MX4009CD Multiplexer configuration

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

I have two Genex MX4009CD Multiplexers connected together. How can I call up cameras according to multiplexer they are connected to?

Product Line

Pelco Cameras

Environment

Genex MX4009CD Multiplexer

Cause

Camera addresses are configure through the KBD4000 keyboard dip switch.

Resolution

CAMERA ADDRESS MODE
There are two modes for addressing cameras:

  • On the KBD4000 Keyboard, set switch 7 OFF if you want to address cameras in groups of 9 according to the multiplexer to which they are connected. For example, multiplexer 1, cameras 1-9; multiplexer 2, cameras 1-9 etc. 
  • Set switch 7 ON if you want to address all cameras consecutively from 1-256 for camera keyboard call up.