How can I set Azimuth Zero on Spectra IV Integrated Dome Camera & Esprit Positioning Systems?

Issue

How can I set Azimuth Zero on Spectra IV Integrated Dome Camera & Esprit Positioning Systems?

Product Line

Pelco Cameras

Environment

Spectra IV Series
Esprit Positioning System

Cause

Azimuth is the pan angle from zero to 359 degrees. Azimuth zero is the pan position you specify to be the zero degree point. Azimuth zero is normally set to magnetic north. Once set, azimuth and compass readings are based on the set Azimuth Zero point. Accessing Spectra IV/Esprit Main Menu requires Preset 95 programming option.

Resolution

To configure azimuth zero

1. Use the joystick to position the cursor beside SET AZIMUTH ZERO.
2. Press the Iris Open.
3. Follow directions displayed on the monitor.

To clear azimuth zero

1. Use the joystick to position the cursor beside CLEAR AZIMUTH ZERO.
2. Press Iris Open.
3. Follow the directions displayed on the monitor.