What are the available receiver address options for the CM6800E-48X8?

Issue

What are the available receiver address options for the CM6800E-48X8?

Product Line

Pelco Matrix

Environment

  • CM6800 Matrix Series

Cause

Programming addresses of PTZ's is not allowed past 32.

Resolution

The CM6800E series matrix supports receiver address range of 1~32 addresses. Daisy-chaining is recommended but not always possible. A maximum of 16 receivers can be daisy-chained from each PTZ port. If more than 32 receivers are required for your system, or if you do not want to daisy-chain the receiver connections, use the CM9760-CDU-T.

You can connect up to four CM9760-CDU-T units to the CM6800E (a total of eight in a 96 x 16 system - four connected to each CM6800E-48X8 unit). PTZ-A, B, C, and D data terminals.