How to determine what protocol the CM9760-DMR Data Manager is set for

Issue

How to determine what protocol the CM9760-DMR Data Manager is set for.

Product Line

Pelco Matrix

Environment

CM9760-DMR
Spectra PTZ camera

Cause

Switch the CM9760-DMR to P or D protocol based on the physical setup. The P protocol merges PTZ commands from CM9700-CC1 units and in D protocol it allows to connect D protocol units (DX7100, DX7000, CM6800, and CM6700).

Resolution

To determine what protocol the CM9760-DMR switches are set for, look at Dip Switch 7 on the mode switch bank. For D protocol turn dip switch 7 ON (Up), for P protocol turn dip switch 7 OFF (Down). Please reference the link provided for visual reference to the dip switch locations and setup.