Which communications port on the CM9760-CXTA Coaxitron Translator is used to connect to a third-party DVR?

Issue

Which communications port (IN port or OUT port) is used to connect to a third-party DVR?

Product Line

Pelco Matrix

Environment

CM9760-CXTA Coaxitron Translator
Third-party DVR

Cause

The IN port is the data connection to which all controllers must interface. The OUT port is used to connect, daisy-chain or cascade two CXTA units together.

Resolution

Use the RS422, RJ45 connector located on the rear of the CM9760-CXTA Coaxitron Translator  which is labeled IN, all controllers must interface using this port.