Network cable type to connect an IP110 Camclosure

Issue

Which network cable should be used to connect an IP110 Camclosure?

Product Line

Pelco Cameras

Environment

  • IP110 Series
  • Straight Cable "or" Cross Over Cable

Cause

Network cable recommended for IP110 installation.

Resolution

The IP110 Camclosure with CAT5 or better will autosense and work with either a cross over or straight cable. The port is an RJ-45 connector for 100Base-TX.