What are the bit rates for the Spectra IV IP Dome System?

Issue

What are the bit rates for the Spectra IV IP Dome System?

Product Line

Pelco Cameras

Environment

Spectra IV IP Dome System

Cause

Configure camera's image quality settings per available bandwidth

Resolution

Primary stream is MPEG-4 - 30 IPS, 2 Mbps
Secondary stream is MPEG-4, 1 Mbps

 
MPEG-4 IMAGE QUALITY
The following are the available MPEG-4 image quality settings:
• HIGH-Multicast (default): 30 ips, 4CIF resolution video stream that can be sent to many users.
• LOW-Multicast: 30 ips, CIF resolution video stream that can be sent to many users.
• HIGH-Unicast: 30 ips, 4CIF resolution video stream that can be sent to up to five users.
• LOW-Unicast: 30 ips, CIF resolution video stream that can be sent to up to five users