How to set the ANALOG OUTPUT for a XMUX2 on a DS Xpress to a static multiplexed view.

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

How to set the ANALOG OUTPUT for a XMUX2 on a DS Xpress to a static multiplexed view.

Product Line

Pelco Video Management

Environment

DS Xpress
XMUX2

Cause

View the analog output with multiple cameras and a set dwell time.

Resolution

  1. Open DS Admin, log in with your credentials.
  2. Click on the Plus next to your system.
  3. Click on the Plus next to VAU
  4. Click on the Plus next to your VAU's name
  5. Click on the Plus next to Analog Outputs.
  6. Select OUTPUT 1 and set it to manual and check box for run defined tour.
  7. Pick your view, and drag cameras onto each pane.
  8. Once complete, click Save Multi View.
  9. On left side, drag your newly saved view into the middle box which is titles Tour.
  10. Delete all other tours in the Tour box.
  11. Set dwell time higher than 60.
  12. Check monitor to see if it took the new monitor setup.

DS Operation/Configuration Manual  See page 18.