Will Axis IP cameras work with the DX8100?

Issue

Will Axis IP cameras work with the DX8100?

Product Line

Pelco Video Management

Environment

DX8100 Series Hybrid Video Recorder
Axis IP camera

Cause

The interface was written using VAPIX ®Application Programming Interface (API) version 2.0 (Firmware 4.xx)

Resolution

The DX8100 has been tested to work with the Axis Model 211 and 232D network cameras. The DX8100 version 2.0 interface is designed to work with Axis standard definition cameras.