What ports are required to connect to DVX500 using DS Control Point?

Issue

What ports are required to connect to DVX500 using DS Control Point?

Product Line

Pelco Video Management

Environment

DVX500
DS Control Point

Cause

Specific network ports need to be open for client software to communicate with DVX500.

Resolution

The following ports need to be open:
 
445 TCP+UDP for FLTime Time Sync (Optional)
1433 TCP     Off-box SQL Server
1434 UDP    Off-box SQL Server,
18772 TCP Used to deliver DS/DVX Video to a network client.