How to connect a KBD300A keyboard to a DX4500/DX4600 Series HVR.

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

How to connect a KBD300A keyboard to a DX4500/DX4600 Series HVR.

Product Line

Pelco Video Management, Pelco Matrix

Environment

  • KBD300USBKIT
    • Belkin adapter
    • PV140
  • KBD300A v5.7 or higher
  • DX4500/DX4600 DVR v1.3 or higher

Cause

Use the KBD300A keyboard to control PTZ cameras attached to the DVR.

Resolution

Installing the KBD300A on a DX DVR Series unit:
 
  1. Open the DIP switch cover on the KBD300A
  2. Set dip switches 6 and 7 to the ON position, and set all other switches to the OFF position.
  3. Close the DIP switch cover.
  4. Connect an RJ-45 cable (supplied) from the KBD300A to the RJ-45 wall block.
  5. Open the cover of the RJ-45 wall block, and wire power from the wall block transformer to pins 3 and 4 on the wall block.
  6. Wire the wall block to the appropriate terminals on the PV140 adaptor.
    1. Connect terminal 1 (TX+) on the wall block to RDB+ on the USB adaptor.
    2. Connect terminal 2 (TX-) on the wall block to RDB- on the USB adaptor.
    3. Connect terminal 7 (RX-) on the wall block to TDB- on the USB adaptor.
    4. Connect terminal 8 (RX+) on the wall block to TDA+ on the USB adaptor.
  7. Close the cover of the RJ-45 wall block.
  8. Connect the USB adaptor to a USB port on your DX DVR Series unit.
  9. View LL#10203 for KBD300A w/KBD power supply distance to KBD300USBKIT



Figure 1. DX Wiring Diagram

 

Related Articles:

How to update the software/firmware of the DX4500/DX4600.