How do you adjust video settings on a Sarix IX series network camera?

Issue

How do you adjust video settings on a Sarix IX series network camera?

Product Line

Pelco Cameras

Environment

Sarix IX Series

Cause

Change the camera's general image settings for the camera location.

Resolution

  1. Open the web browser.
  2. Type the camera's IP address in the browser address bar.
    NOTE: If you do not know the camera's IP address, you can locate it using the Pelco Device Utility software.
  3. Click the Login button in the navigation bar; a dialog box appears.
  4. Type the Admin ID and password.
    NOTE: If you are logging on to the camera as the administrator for the first time, the default User ID and Password are admin (all lowercase).
  5. Click Log in.

Refer to the Imaging Tab section on page 34 in the Installation/Operation IX Series manual for more information on video settings.