IMSOC10 video is too dark

Issue

IMSOC10 video is too dark. What can I do to improve it?

Product Line

Pelco Cameras

Environment

IMS0C10

Cause

Adjust camera settings to camera's location condition.

Resolution

Color camera only: Set the Night Max Exposure Time. 

  1. Log in to the IMS0C10 camera.
  2. Navigate to Imaging Tab and select Exposure.
  3. Adjust the Night Max Exposure Time.

* Night Max Exposure Time:  This setting controls the maximum time in milliseconds that an image is exposed during dim light, such as nighttime conditions. Increase this time to increase the light sensitivity of the    camera. the exposure range is 1 to 500 msec; the default setting is 120 msec.