Issue
Is there a cover plate for the rear opening of the IWM-GY mount?
Product Line
Pelco Cameras
Environment
IWM-GY mount
Cause
Use the block-off plate to close up any opening beside holes for wiring.
Resolution
Part number 9204106COMP Block off plate. This part is used with the PA402 Pole Adapter mount but may be used for the rear opening of the IWM-GY mount. There are two conduit knock-outs that are 1/2" -3/4".
* Part numbers are subject to change without notice.