Issue
- No coaxitron PTZ control of Spectra from DSSRV with ENC5416.
- How do you connect a CM9760-CXTA to a DSSVR system?
Product Line
Pelco Video Management
Environment
- DSSRV
- ENC5416
- CM9760-CXTA
- Spectra Series PTZ
Cause
ENC5416 analog encoder does not support coaxitron protocol. The ENC5416 only supports Pelco D No Parity protocol.
Resolution
DSSRV with ENC5416 requires the CM9760-CXTA to support Pelco Coaxitron control.
Note: Looping video to three or more devices can cause PTZ control to malfunction, when configuring for the first time setup DS system and CM9760-CXTA as illustrated.
Connection illustration:
-
Make all necessary connections with system powered off.
-
Change the Dip switch on the CM9760-CXTA.
-
Connect the Data cable between the CM9760-CXTA and the ENC5416.
Related articles:
Configure a DSSRV for PTZ control using the ENC5416.