The buttons/icons on the DX Series Client are misplaced and are not scaled correctly.

Issue

The DX Series Client is displaying the buttons/icons incorrectly and are misplacing them where the text boxes are located.

Product Line

Pelco Video Management

Environment

DX Series Client v1.0.1.0010
Microsoft Windows 7

Cause

The text size in Microsoft Windows 7 OS is configured to medium-125% , the DX Series Client is unable to rescale to match.

Resolution

Change the text size to smaller-100%(default).
  1. Right-click on the Windows 7 desktop and select Personalize.
  2. Click on the Display link at the bottom left of the window.
  3. Select the smaller-100%(default) radio button and Apply to save setting.