What is the size of the Camera lens combination that will fit in the HS8080?

Issue

What is the size of the Camera lens combination that will fit in the HS8080?

Product Line

Pelco Cameras

Environment

HS8080

Cause

Require the dimension of the housing to purchase the correct camera and lens size.

Resolution

EH8080 Maximum Camera and Lens Size (including BNC connector) up to:

3.50" H x 3.00" W x 9.75" L
(8.99 x 7.62 x 24.77 cm)