What are the power requirements of the CM9760-KBD Intelligent Keyboard?

Issue

Power supply is needed for the CM9760-KBD Intelligent Keyboard?

Product Line

Pelco Matrix, Pelco Transmission & Power

Environment

CM9760-KBD Intelligent Keyboard

Cause

Power supply is needed for the CM9760-KBD Intelligent Keyboard.

Resolution

The CM9760-KBD Intelligent Keyboard includes the power supply module.  The PS01-3002-9015G (with region power cord) is a universal power supply that operates on 90-264 VAC at 1.0A MAX, 50/60 Hz input power and supplies 15 VDC at 2A to the CM9760-KBD.

Note: The KBD-KIT will not power the keyboard.