Will the TXB-IP or TXB-N IP converter work in the Spectra III back box?

Issue

Will the TXB-IP or TXB-N IP converter work in the Spectra III back box?

Product Line

Pelco Cameras

Environment

TXB-IP
TXB-N
Spectra III

Cause

The TXB-IP and TXB-N allows an existing Spectra IV camera system to retain all of its current system and analog capabilities while adding IP connectivity.

Resolution

No. The TXB-IP and TXB-N will not work in the Spectra III back box.