Issue
Are the CM9770-VCC and CM9770-VMC cards the same?
Product Line
Pelco Matrix
Environment
- CM9770-VCC
- CM9770-VMC
Cause
Understand the function and purpose of the two cards for installation.
Resolution
No. The CM9770-VCC Video camera card is capable of accepting up to 32 camera inputs only; also requires a rear panel card (CM9770-DFC, CM9770-DFL, or CM9770-RPC). The CM9770-VMC Video monitor card providing 16 monitor outputs only; requires CM9780-RPM.