Camera and Mount option for Inside Corner applications

Issue

What Pelco camera can I use in an elevator?

Product Line

Pelco Cameras

Environment

  • Inside/Inward corner mounting for IS50/IS51
  • IS50/IS51
  • IS50-CM

Cause

Mounting a camera and housing to inward/inside corner application.

Resolution

The IS50-CM corner mount is specifically designed for use with IS50/51 Series Camclosure 2 dome cameras. The corner mount allows the dome to be installed flush to a corner.

Click here to review I/O manual of IS50-CM