Issue
How long will I/NET 2000 be sold?
Is I/NET 2000 still supported?
Product Line
TAC I/NET
Environment
All Revisions of I/NET 2000
Cause
The last release of I/NET 2000 was Revision 2.34 which was released in April 2003. Microsoft has announced that it will terminate all Windows® 98 support in 2006.
Resolution
As of January 1, 2006, support for I/NET 2000 is no longer available. Please review the following Customer Advisory available on The Exchange Download Center which details support information for I/NET 2000.
All I/NET 2000 customers should upgrade to the latest revision of I/NET.