Cannot combined multiple CM6700-MXB Matrix Switchers into a single system

Issue

Can multiple CM6700-MXB Matrix Switchers be combined into a single system?

Product Line

Pelco Matrix

Environment

CM6700-MXB2 Series
CM6700-MXB4 Series

Cause

The CM6700 Matrix switching unit is designed to be remotely operated from desktop keyboards (KBD100, KBD200A, KBD300A) and as standalone unit.

Resolution

No. The CM6700-MXB2/4 Matrix Switchers will only operate as standalone units. If expansion beyond 32 cameras or 4 monitors is needed, look at  the CM6800E Series Matrix Switcher.