Which ports are powered for local keyboards on the CM6800E-48X8 Matrix Switcher?

Issue

Which ports are powered for local keyboards on the CM6800E-48X8 Matrix Switcher?

Product Line

Pelco Matrix

Environment

CM6800E-48X8 Matrix Switcher
KBD100
KBD200A
KBD300A
 

Cause

Plugged keyboard to any other ports beside port 5 and 6 will not power the keyboard.

Resolution

Ports 5 and 6 on the CM6800E-48X8 Matrix Switcher will supply power for local keyboards.


For instructions with illustration, see page 19 of the CM6800E-48X8 Matrix Switcher Installation and Operation Manual