Can the DX4700/DX4800 Series Hybrid Video Recorders (HVR) be administered remotely?

Issue

Can the DX4700/DX4800 Series Hybrid Video Recorders (HVR) be administered remotely?

Product Line

Pelco Video Management

Environment

DX4700/DX4800 Series HVR

Cause

Configure the DX4700/DX4800 Series recorder at remote site.

Resolution

Yes, using the DX Series Client. There are some setup features which must be configured at the server, configuring the server date/time and network information must be performed locally.