Configure Spectra IV IP H.264 camera to be an all-color camera

Issue

How do I configure a Spectra IV IP H.264 camera to be an all-color camera without black/white operation?

Product Line

Pelco Cameras

Environment

Spectra IV IP H.264

Cause

Keep the camera in color operation at night time.

Resolution

  1. Connect to the Spectra IV IP using the web interface by navigating to the IP Address of the camera in your web browser.
  2. Log in with an administrator account (default username=admin password=admin)
  3. Go to Settings>Camera Configuration>OSD camera menu appears.
  4. Choose Dome Settings>Camera
  5. Scroll down to Ir cut filter, press iris open icon
  6. Change setting to IN
  7. Press Iris open
  8. Scroll down to exit and press iris open.