Does the DX4700/DX4800 Series Hybrid Video Recorder have a bandwidth throttle feature?

Issue

Does the DX4700/DX4800 Series Hybrid Video Recorder have a bandwidth throttle feature?

Product Line

Pelco Video Management

Environment

DX4700/DX4800 Series Hybrid Video Recorder (HVR)

Cause

Limit the amount of network resources allocated to client connections.

Resolution

Yes. The bandwidth throttle can be adjusted under the Network settings in the DX4700/DX4800 Server. Follow the following steps to configure the bandwidth throttle:
 
  1. Click on the setup icon.
  2. Go to the System icon.
  3. Go to Network. The bandwidth throttle is available.
    NOTE: The default bandwidth throttle is 100 Mbps.