Are the SEB5100's compatible with the NSM5200 recorders?

Issue

Are the SEB5100's compatible with the NSM5200 recorders?

Product Line

Pelco Video Management

Environment

Endura SEB5100 Series
Endura NSM5200 Series

Cause

The SEB5100 and NSM5200 are two different platforms and will not communicate with each other.

Resolution

The SEB5100's are only compatible with NVR5100's and DVR5300 recorders.