What PTZ control protocols do the Pelco Fiber modules support?

Issue

What PTZ control protocols do the Pelco Fiber modules support?

Product Line

Pelco Transmission & Power

Environment

Pelco Fiber Series

Cause

For the PTZ camera and fiber to communicate both devices need to have the same PTZ control protocol.

Resolution

Pelco Fiber Modules support the following protocols:
RS-232, RS-422, RS-485 (2-wire/4-wire), Manchester, Coaxitron and Bi-Phase Communication.
 
Check the spec sheet for the specific fiber model features such as protocol support and distance limitation: Fiber products spec sheets.