NOTICE
DISCONTINUED PELCO PRODUCT.This product has been discontinued. For further information please visit pelco.com/support/discontinued-products
Issue
How to program and run a Preset Tour on the DX7100 (DVR)?
Product Line
Pelco Cameras, Pelco Video Management
Environment
- DX7100 Series DVR
- PTZ camera
Cause
For PTZ (Pan Tilt Zoom) camera to perform a sequential movement, the preset and tour settings need to be configure.
Resolution
Preset Tours:
A preset tour is a programmed sequential execution of multiple preset positions.
HOW TO PROGRAM A PRESET TOUR
- Click the PTZ button in the DISPLAY mode. The PTZ mode appears.
- Click PRESET. The preset bar appears.
- Select a camera by moving the mouse pointer to the desired camera view and clicking the left mouse button.
- Click the TOUR button to turn on tour programming.
- Click the SET button to turn on preset programming.
- Click PRESET buttons in any sequential order to program a tour.
- To stop programming the preset tour, click the TOUR button.
HOW TO RUN A PRESET TOUR
- Click the PTZ button in the DISPLAY mode. The PTZ mode appears.
- Click PRESET. The preset bar appears.
- Click TOUR.
- Set the time to switch between presets. The time selection buttons are located above the preset buttons.
- Click MOVE. The preset tour starts. The number in the preset button turns orange to indicate which preset the tour is on.
- To stop the tour click MOVE.
- Click TOUR to exit touring.
HOW TO CLEAR A PRESET TOUR
- Click the PTZ button in the DISPLAY mode. The PTZ mode appears.
- Click PRESET. The preset bar appears.
- Click TOUR.
- Click CLEAR. The preset tour is now cleared. A preset tour must be cleared before a new preset tour can be programmed.
- Click TOUR to exit touring.