Do the connection cables for the ENC5416/ENC5516 come with the ENC5400-4PORT/2PORT card?

Issue

Do the connection cables for the ENC5416/ENC5516 come with the ENC5400-4PORT/2PORT card?

Product Line

Pelco Video Management

Environment

  • ENC5400-4PORT
  • ENC HDMI Cable
  • ENC5416
  • ENC5516
  • DSSRV

Cause

Require cable to connect the ENC5416/ENC5516 encoder to the Digital Sentry SRV system.

Resolution

Yes, the connection cables for the ENC5416/ENC5516 come with the ENC5400-4PORT or ENC5400-2PORT.
If needed, the part number for the cables = ZSPENC5400-0031 but may only be ordered with KIT PN# ENC5400-CBUPKIT. Qty 2 are in the kit.