Use Pelco Device Utility 2 software to detect Pelco network IP cameras.

Issue

  • Do Pelco have a software application to detect Pelco network IP cameras?
  • Link to download Device Utility 2

Product Line

Pelco Cameras

Environment

  • IP110 Series
  • Sarix Series
  • Spectra IV IP
  • Spectra HD
  • Spectra Mini IP
  • Esprit SE IP
  • ExSite IP Series

Cause

Discover all Pelco IP cameras on the same network for configuration and maintenance.

Resolution

Yes. The Device Utility 2 is a software application that you can install on your PC and MAC to detect any Pelco IP cameras installed on your network. The Device Utility 2 software enables efficient advanced configuration, maintenance, and troubleshooting of supported Pelco network devices. This software helps you fine-tune your devices and network. The Device Utility 2 software supports the following functions:
  •  Checking overall system attributes
  •  Updating device software, individually or by groups of devices
  •  Checking device status
  •  Identifying devices
  • Adding and removing devices
  • Viewing devices by groups
  • Generating reports
  • Setting up system preferences

Download the Device Utility 2


Click here for the Installation/Operation Device Utility 2 Software.