Can KBD300A program and recall PTZ presets when used with the DX4500/4600 Series DVR?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

Can KBD300A program and recall PTZ presets when used with the DX4500/4600 Series DVR?

Product Line

Pelco Video Management

Environment

KBD300A
DX4500/DX4600 Series DVR

Cause

Program and activate a present from KBD300A keyboard.

Resolution

Yes. The KBD300A is capable of programming and calling PTZ presets when connected to the DX4500/4600 Series DVR.