How to set-up a new CM9765 Matrix Switcher

Issue

How do I set up the new CM9765 Matrix Switcher?

Product Line

Pelco Matrix

Environment

CM9765 Matrix Switcher system

Cause

New CM9765 Matrix Switcher out of box and need instruction on how to set up.

Resolution

1. Unpack and inspect all equipment, and verify delivery according to the packing slip.

Before shipping, Pelco connects, tests, and programs each system according to the individual sales order. Contact Pelco immediately if
There is any discrepancy in the equipment that you receive.
CM9700-CC1
The following items are supplied with the CM9700-CC1:
• 1 CM9700-CC1 unit, with front rack ears installed
• 1 120 VAC, 60 Hz power cord (USA standard)
• 1 230 VAC, 50 Hz power cord (European standard)
• 1 Keyboard, PS/2
• 1 PS/2-to-AT keyboard adapter
• 1 RCA-to-BNC adapter
• CM9700 Resource CD (includes the CM9700-MGR software)
• BNC extraction tool
• 4 Rack mount screws, 10-32 x .750-inch, Phillips, pan head with washers
CM9765-MXB
The following items are supplied with the CM9765-MXB:
• 1 CM9765-MXB matrix bay, with front rack ears installed
• 1 CM9765-MXB mounting baffle, with front and rear rack ears installed
• 1 120 VAC, 60 Hz power cord (USA standard)
• 1 230 VAC, 50 Hz power cord (European standard)
• 1 RJ-45 reversed data cable
• 1 Sheet of camera number labels (these can be affixed to the BNC cards to correspond to camera input numbers)
• 16 Screws and washers for mounting the bay
2. Keep all manuals and cabling with their associated equipment.
3. Locate the following documents:
• System 9765 Port Assignments Sheet. This document contains specific information about your system. All System 9765s are
Preprogrammed based on your system order.
• System 9765 manual binder.
NOTE:
The appropriate number of CM9765-VCC cards (camera cards), CM9765-VMC cards (monitor cards), and associated rear panels are
Added to your system according to your system order.
MOUNTING
Install System 9765 in an EIA-standard 19-inch (48.26 cm) racks.
CM9765-MXB
1. Install the CM9765-MXB mounting baffle first. The mounting baffle uses 1 rack unit (RU), and it has front and rear mounting ears, which are attached to the front and rear mounting racks.
The rear mounting brackets are adjustable to allow for different depths of cabinets.
The mounting baffle provides the following functions:
• The mounting baffle helps to direct the heat from a lower matrix bay (or other equipment) toward the rear of the mounting baffle,
Instead of allowing the heat to flow up into the matrix bay.
• The mounting baffle supports the weight of the matrix bay.
• The matrix bay is easier to install when it is sitting on top of the mounting baffle.
2. Install the CM9765-MXB matrix bay on top of the mounting baffle. In a single-bay installation, always leave 1 RU of space above the matrix bay for airflow.
In a multiple-bay installation you do not need to leave additional RUs open between units. However, you must always leave 1 RU of space above the upper bay.

For further instructions with illustrations, see the CM9765 Installation Manual starting on page 10