Configure the Recording Setup on the DX4500/DX4600 Series digital video recorder

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

How to set up Record Settings on the DX4500/DX4600 Series digital video recorder?

Product Line

Pelco Video Management

Environment

  • DX4500 DVR
  • DX4600 DVR

Cause

Configure Recording Setup.

Resolution

  1. On the front panel of the recorder or on the remote control, press the up/down arrow buttons to highlight Record. Using the mouse, click Record. The record option is highlighted and the property settings are displayed.

    Figure 20. Record Option Settings

     
  2. To configure a Record Setting, do the following:
    1. On the front panel or remote control, press ENTER. Press the left/right arrow buttons to select the resolution, quality, image rate, pre-alarm, and post-alarm fields, and press ENTER. Then press the up/down arrow buttons to set the settings for a channel. Using the mouse, click the settings.
    2. Repeat step 2a for additional channels.

For complete procedure see pages 35-49 of the DX4500/DX4600 Operation and Programming Manual.

Also see Lessons Learned Article #9268.