How to install the VAU only portion of the software for a enterprise system running 7.0.24.

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

How to install the VAU only portion of the software for an enterprise system.

Product Line

Pelco Video Management

Environment

Product: DSNVR / 7.0.24 / DIGITALSENTRY Peripheral equipment: Distributed system, 1DMS, multiple VAU's

Cause

The customer is installing a new VAU and is trying into install the VAU only part of 7.0.24 software suite.
The problem is that there is no option for Enterprise/Distributed systems in the normal installer.

Resolution

To function properly the DS NVR which is part of an enterprise system, needs to have the VAU only software installed to work.

To install the VAU only portion of the DS software for 7.0.24, you need to install the software as VAU/DMS or any component of an ENTERPRISE SYSTEM, do the following.

  1. Unzip the 7.0.24 package.
  2. Go to ISSetupPrerequisites
  3. Go to the {AE1B405D-93B8-4309-8E3E-C7D99B755EAD}
  4. Then Click Setup
  5. Click Next
  6. Select Distributed System
  7. Then select either VAU/DMS/VSAN
  8. Then continue the installation until it finishes.